AMERICAN BRIGHT OPTOELECTRONICS 

Leading LED Suppliers Seeking Unusual Quality and Service 

 

In 1995, Bright established American Bright Optoelectronics Corporation in Southern California to create a qualified, responsive source to the rapidly growing market for LED’s in the North America market.

 

With the same philosophy that Bright has continually invested in the expansion of their research and development, manufacturing and customer service capabilities, American Bright is capable of responding to the needs of the customers on a domestic basis. This is achieved through a growing network of authorized sales representatives, applications staff and qualified distributors. Leveraging our ability to communicate immediately with the factory and with customers and affiliates around the world, and through the further growth of our automated production lines, American Bright is positioned to answer the most demanding needs of our customers. Our manufacturing techniques are highly proficient, assuring a level of quality and uniformity that the market has come to expect in such devices.

 

Top Seller

AMERICAN BRIGHT OPTOELECTRONICS

AB-GES Series 280 x 24 mm Linear 120V 12 W (3000K 1100 lm min) LED Light Engine

Mfr Part#:AB-GES-L28...
  

RoHS compliant

From as low as   $19.35 USD

All AMERICAN B... Products

By Category

 

Stay in touch with the latest news...