From it’s inception in 1983, Tianma has continuously pursued innovation and product improvement permitting them to maintain an un-rivaled position as a leading international supplier of Liquid Crystal Displays. Renown as the largest manufacturer of passive and monochrome LCD's of continental China, the company now occupies a territory of almost 1.2 million square feet. Ninety percent of which is dedicated to manufacturing space.
Tianma has an unwavering commitment to excellence with regards to the company’s 4000 plus employees. Since 1996, its R&D Department has been officially recognized as one of the Top 3 R&D Centers of China’s Guandong Province. It is recognize as "Best in R&D" since year 2000 in Shenzhen City.
Tianma's long-term success is inexorably linked to the technical expertise of its R&D team. The company’s’ displays meet specific challenges of operation - without compromise - under the most arduous of field conditions. Tianma is also a fully integrated manufacturer focused on "highest quality for the best cost". Tianma has a new 4.5 Gen TFT factory in place, and is currently manufacturing their own TFT line.
Tianma produces displays resistant to extreme temperatures from -50 to +90 C at low voltages. They also offer a wide range of conventional and special Liquid Crystal Technologies, such as: TN, HTN, ETN, BMTN, STN, FSTN, FFSTN, NFSTN, DSTN, ESTN, ECB, FSLS, LFSL, Multi-Color TN, Color STN, and most recently TFT.
Tianma Microelectronics now proudly celebrates two remarkable decades of its history. From the foundation in 1983, proactive pursuit of innovation and continuous product improvement enabled Tianma to maintain its un-rivaled position as a leading international supplier of Liquid Crystal Displays.
TM104SDH01 is a Active color TFT display, which has a diagonal size of 10.4" with the resolution of 800(RGB) x 600 . It interfaces with LVDS 6 bits. It is a a-si TFT Technology type, TM with Normally White display mode.
Features :
- Size : 10.4"
- Resolution : 800(RGB) x 600
- Interface : LVDS 6 bits
- Color Depth : 262k
- Technology Type : a-Si
- Pixel Pitch (mm) : 0.264 X 0.264
- Pixel Configuration : R.G.B. Vertical Stripe
- Display Mode : TM with Normally White
- Surface Treatment (Up Polarizer) : Anti Glare(3H)
- Surface Treatment(TSP) : Anti-glare type (3H)
- Viewing Direction : 12 o’clock
- Gray Scale Inversion Direction : 6 o’clock
Mechanical Characteristics :
- LCM (W x H x D) (mm) : 236.00 x 176.90 x 5.60
- Active Area(mm) : 211.20 x 158.40
- With /Without : Without TSP
- Weight (g) : 288
To learn more about TM104SDH01 product family, Click Here