What is Luxeon®?
LUXEON® Emitters are the highest flux LEDs in the world, delivering the brightest solid-state lighting solutions available. Luxeon Emitters can produce more than 45 lumens per Watt, and LUXEON® Emitters are 20 to 40 times brighter than standard LEDs. Luxeon is an optimum light source for a wide variety of applications.
Lasts longer than any other light source—more than 10 years
LUXEON® contains solid-state technology made in Silicon Valley using technology similar to those used in the latest microprocessors. Unlike typical conventional light sources, LEDs do not fail catastrophically; meaning they do not dramatically burn out and cease to function. In many applications LUXEON® will last for more than 10 years of operation.
Reduced maintenance costs
Since LUXEON® lasts at least 10 times longer than a typical light source, there is no need to replace the light source, thereby reducing or even eliminating ongoing maintenance costs and periodic relamping expenses. Be the environmental solution. Luxeon is more energy efficient than incandescent and halogen light sources, and is fast approaching the efficiency of fluorescents.
Vivid saturated colors—without filters
LUXEON® requires no filters to create colored light, resulting in deeper saturated colors without wasted light. Deep reds, greens, blues and other colors can be produced directly from this solid-state source.
Directed light for increased system efficiency
LUXEON® light sources are small, directional, pinpoints of light. This size and directionality result in highly controllable optical systems, resulting in no wasted light.
Robust, solid-state lighting
LUXEON® high-power light sources are solid-state devices. There are no moving parts, nothing to break, rupture, shatter, leak or contaminate the environment.
Dynamic color control, white-point tunable
The vivid, saturated colors of LUXEON® enable a wide color gamut of saturated static and dynamic lighting effects. From tunable white to a single light capable of digitally producing any color under the rainbow, Luxeon offers new dimensions to the lighting world.
Fully dimmable—without color variation
LUXEON® light sources are fully dimmable without sacrificing any characteristics of the light.
No mercury in the source
Unlike fluorescent sources, Luxeon contains no mercury.
No heat or UV in the light beam
No harmful ultraviolet rays or infrared heat is contained in the LUXEON® light beam.
Cold start capable
LUXEON® has no ignition problems in cold environments—even down to -400C.
Low voltage DC operation
LUXEON® is a current driven solid-state device, operating at voltages as low as 3.5 VDC.
|