FTM / AI & Edge Solutions / Future Electronics — Matter Protocol
Read this to find out about:
In the consumer device world, the Matter protocol is exciting huge interest because it holds out the promise, finally, that all smart devices in the home can respond to commands from a single controller or app.
The vision of the Connectivity Standards Alliance (CSA), the 550-strong consortium of consumer device manufacturers and chip companies which has defined the Matter standard, is that controlling smart home devices will become simple, reliable and secure: the user’s preferred app, such as Amazon’s Alexa, Google Home or Apple’s Siri, will be able to control any Matter-certified device in the home, no matter which brand manufactured it. The Matter protocol will support a variety of common smart home products, including lighting and electrical devices, HVAC controls, window coverings and shades, safety and security sensors, door locks, media devices including TVs, controllers as both devices and applications, and bridges, shown in Figure 1. And commissioning a new device into a Matter network will, according to the CSA, be as simple as capturing a QR code on the user’s network-connected smartphone, or tapping the phone to make an NFC connection.
As the CSA website says, ‘Matter is the seal of approval that says smart devices work reliably together, taking the guesswork out of the purchasing process. That trust allows you to choose from a wider range of the brands you love and brings you the comfort of a secure and seamless connected home.
Fig. 1: Devices carrying the Matter logo can be relied on to communicate with each other.
The CSA Matter initiative is backed by the giants of the consumer electronics industry, including Apple, Samsung, Google, Amazon, Signify, LG, Huawei, and Oppo: it seems unlikely that any rival technology will emerge to compete with it. So designers of home automation products are soon, if not already, likely to be tasked with implementing Matter technology into new product designs. The designers might also need to bolt Matter support onto existing products.
Before embarking on a Matter design project, engineers can learn from the early experience of Future Electronics. The Centre of Excellence (CoE) in embedded engineering, based in Gdansk, Poland, has worked hand-in-hand with chip companies STMicroelectronics and NXP Semiconductors to develop Matter-compliant prototypes and production-ready designs for customers in the lighting industry. The CoE experience shows that, while the Matter protocol largely lives up to its promise of being a plug-and-play technology for developers, there are some important hardware and software considerations to take into account.
Essential features of the Matter protocol
According to the CSA, the Matter protocol is ‘a unified, open-source, application-layer connectivity standard’, shown in Figure 2. This means that it is dependent on, and separate from, physical transport networks that carry data. By design, the Matter protocol is compatible with Thread, Wi-Fi® and Ethernet transport networks. A Bluetooth® Low Energy connection may be used for pairing an end device with a Thread or Wi-Fi network, but may not be used for transporting Matter data.
The standard uses the Internet Protocol version 6 (IPv6) as the common language of Matter devices.
Fig. 2: The architecture of Matter technology, showing that it operates as an application layer separate from the physical transport network.
The Matter specification details everything necessary to implement a Matter application and transport layer stack. Source code for the Matter project is available for download from the CSA GitHub page at github.com/project-chip.
The goal of the Matter development project was to create a protocol that would be widely deployed across a broad range of smart home devices, not only those with substantial computing capability, such as Wi-Fi routers or smart TVs, but also products such as smart light bulbs, doorbells and light switches that are typically based on a microcontroller.
As the Matter GitHub page says, ‘The protocols are broadly deployable and accessible, by leveraging IP and being implementable on low-capability devices.’ The Matter specification also supports the Linux® operating system, for devices with higher compute capability, and the FreeRTOS operating system for resource-constrained devices.
Current extent of Matter support from SoC manufacturers
Many implementations of Matter technology will be made in a microcontroller environment. In theory, an OEM can choose to port the Matter software to any system-on-chip (SoC) of choice, the protocol is meant to be hardware-agnostic, although the specification requires over-the-air update capability, which itself calls for external Flash memory.
But as of the start of 2024, some MCU manufacturers provide extensive support for Matter technology; others, none at all.
Why does this matter? In theory, after all, a designer is able to download the Matter source code from github.com/project-chip to their target hardware, the core of the protocol software can be optimized to fit almost any MCU with at least 500 kbytes of available storage capacity.
In practice, this is very hard for any engineer who is not already a Matter expert to do. Far better is to use the Matter software development kit (SDK) compiled for any given MCU by that MCU manufacturer. But then designers will run into the problem of the scarcity of Matter-compatible MCUs. One manufacturer that has moved quickly to build Matter compatibility into its MCU products is STMicroelectronics.
The ST SDK provides an optimized and streamlined implementation of the Matter protocol for a 32-bit MCU environment through its X-CUBE-Matter software development kit. ST is also progressing fast with work to build out the support for Matter across the entire STM32 ecosystem. For instance, design implementation requires a detailed description of the device. This may be done with the Zigbee Cluster Library (ZCL) Advanced Platform (ZAP) tool. The CSA is the publisher of the Zigbee standard as well as the Matter protocol.
The ZAP tool enables the developer to:
ST is integrating the ZAP tool into the STM32CubeMX middleware, providing a streamlined development environment for Matter implementation.
Common challenges encountered in Matter design projects
The Future Electronics CoE in Gdansk has gained considerable experience in embedding Matter capability into smart lighting products, using the STMicroelectronics STM32WB5MMG 2.4 GHz wireless MCU module as the hardware basis, shown in Figure 3. This ST module supports both Thread and Bluetooth Low Energy networking. The CoE experience has revealed that, while the Matter specification is designed for ease of use both by the developer and the end user, there are some pitfalls of which engineers need to be aware.
Fig. 3: The STM32WB5MMG module is supplied in a compact 7.3 mm x 11 mm x 1.4 mm 86-pin LGA package.
Memory usage: the Matter protocol has a tendency to be a RAM hog. This drawback of version 1.0 was improved in v1.1 of the Matter specification, and future releases can be expected to be better still. But it is important for designers to carefully specify the RAM capacity in the chosen hardware target.
An effective way to reduce dependence on the MCU RAM resource is to implement the Matter protocol’s cryptography and other security functions in an external secure element such as the NXP EdgeLock® SE051H, shown in Figure 4. The SE051H offers extended Matter support, including:
Fig. 4: The NXP OM-SE051ARD-H is an Arduino board-compatible development kit for the EdgeLock SE051H secure element, which integrates NFC functionality to simplify the secure onboarding of Matter devices in the smart home.
Certification: always the bane of embedded development teams lives, and not made easier by the need to validate Matter compatibility separately from the Thread or Wi-Fi certification process, shown in Figure 5.
Fig. 5: The Matter certification workflow for a Thread- or Wi-Fi-compliant device
Use of an STMicroelectronics device such as a wireless MCU from the STM32WB5 family is helpful in this regard: ST publishes a manual on Matter certification, and provides access to third-party support for certification. In addition, some ST devices, including the STM32WB5MMG module, are supplied pre-certified for RF and Bluetooth standards compliance, and its certificates can be passed through to the end product without additional validation.
Nevertheless, every manufacturer of a Matter-certified end product must be registered with the CSA: registration requires payment of a substantial fee. In addition, the CSA supplies certain ID credentials, the Device Attestation Certificate and the Certificate Declaration, via a proxy known as a Product Attestation Authority (PAA). A device ID enables a production unit to be recognized by the Matter firmware.
Procuring these device attestation credentials could prove to be a bottleneck in the development process.
Connectivity: in version 1.0 of the Matter protocol, the CoE encountered problems with intermittent loss of Thread connectivity. There were various causes, including the RAM issue highlighted above. Also, when a Thread device lost power and then re-started, it was required to re-register its security credentials with the host network.
These problems were fixed in the v1.1 release of the Matter firmware. This means that developers should make sure that they are working with the latest release of the Matter specification. The potential for bugs to emerge is not surprising given the short period of time that has elapsed since the release of the first Matter specification. Developers should expect multiple updates to appear over the coming months and years.
Getting started with Matter design implementation
For MCU-based designs, Matter software support was already, in the first half of 2024, provided in products from STMicroelectronics, NXP, Infineon, Renesas, and Espressif Systems.
Designers who want to get started with a Matter-certified product design would benefit from working with an ST dev kit such as the STM32WB5MM-DK Discovery kit for the STM32WB5MMG module, in Figure 5. The Future Electronics CoE for embedded engineering can provide detailed guidance based on experience in implementing the Matter protocol on the STM32WB5MMG.
Fig. 5: The STM32WB5MM-DK Discovery kit from STMicroelectronics provides a rich environment for developing Matter-certified devices.