Shipping Country
Free shipping within the continental US over $50. Conditions apply
Select Country
Meet your data storage needs with our comprehensive line of memory modules. While memory chips are used in various portable devices like smartphones, tablets, PCs, and media players, flash memory is widely used in BIOS, PCMCIA cards and modems. Whatever your needs, we house several categories of memory devices including FRAM, MRAM, Static RAM, DRAM, EPROM and more. Our search filters help you search by brand or category for convenience.
FLASH is a type of non-volatile Memory device, meaning data is not lost when power is removed. FLASH is the most widely used type of memory device and it is split into two main categories: NOR and NAND. NOR FLASH offers faster read speeds and random-access capabilities, making it suitable for code storage and execution. NAND FLASH, on the other hand, has faster write speeds than NOR and it is typically used to store large data files such as music, movies, pictures, etc. NOR FLASH is available in two formats, Parallel or SPI (Serial Peripheral Interface). Over time, SPI FLASH has evolved into many different subcategories including Multi I/O, Quad SPI, Hyperbus, Octal, Semper, Wide Voltage, etc. NAND FLASH is offered in form of SLC (Single Level Cell) NAND components. But NAND FLASH is largely consumed in form of die. NAND die is used to build storage devices such as USBs, Memory Cards, Solid State Drives, Embedded Multimedia Cards, etc. The NAND die used to build these devices can be TLC (Tri Level Cell), MLC (Multi Level Cell), PseudoSLC or SLC. TLC NAND is the most inexpensive, while SLC NAND has the highest price, the price variance being directly linked to the endurance – how many read and write cycles each type of die can tolerate before it deteriorates. The accepted “rule of thumb” (which can vary based on the application) is that TLC NAND is good for up to 500 cycles, MLC for up to 3,000 cycles, PseudoSLC (or SLC-Lite as it is sometimes called) will work well up to 20,000 cycles and SLC NAND will be good for 60,000 cycles. Future Electronics distributes high quality FLASH devices from world class suppliers. These devices are available on futureelectronics.com in trays, tubes, reels or individual quantities.
Centon Professional Series memory solutions deliver dependable pe...
Infineon offers a comprehensive portfolio of HYPERRAM™/Octal xSPI...
Kingston embedded DRAM components are designed to meet the requir...
Future Electronics introduces Northern Lights, the first of sever...
The Avalanche Development Kit allows developers to quickly protot...
A semiconductor memory chip is an electronic device for data storage which is implemented on a semiconductor integrated circuit. Data is accessed by the semiconductor chip through a binary memory address. If the address of the memory consists of M number of bits, then the address area consists of 2^M addresses per chip. Semiconductor memory chips are designed with a certain word length (which is the number of 1-bit cells that share the same memory address). The amount of data which can be stored in a memory chip defines the number of bits. Through the combination of several integrated circuits, memory may be arranged for a larger word length and/or a larger address space than what is initially offered by the chip.
There are several different kinds of Memory devices suitable for programming at Future Electronics. We stock many of the most common types categorized by several parameters including Nominal Supply Voltage, Temperature Range, Memory Organization, Maximum Access Time, Memory Density, Interface Type, Operating Mode and packaging type, among others. Our parametric filters will allow you to refine your search results according to the required specifications.
Future Electronics has a wide range of programmable memory devices from several manufacturers. Once you decide if you need Battery Backed SRAM, Combo Flash Memory, DRAM, Dual Port Memory, EEPROM, EPROM, FIFO's, Flash Memory, FRAM, MRAM, Non Volatile SRAM, PSD Memory, Static RAM or Volatile Memory, you will be able to choose from their technical attributes and your search results will be narrowed to match your specific memory device application needs.
We deal with several manufacturers such as Alliance Memory Inc, Cypress, Everspin Technologies, Greenliant, Macronix, Microchip, ON Semiconductor, Renesas Electronics, Simtek and STMicroelectronics, among others. You can easily refine your memory product search results by clicking your preferred memory brand from the list of manufacturers below.
All types of electronic devices can use semiconductor memory chips. They can be found in as many fields as: PCs, digital cameras, notebooks, smart cards, aerospace and military system, cellular telephones and smart phones, digital music devices and media players, digital cameras, cellular base stations, black box solutions, book readers, PDAs, power meters, security systems and removable storage devices among other uses. Flash technology can be found in computer BIOS, PCMCIA cards, video game cartridges and modems. Bridges, routers and switches use FIFO memory in communications and networking to hold data packets that are in route to a given destination.
With the FutureElectronics.com parametric search, when looking for the right Memory devices, you can filter the results by category. We carry the following categories of Memory devices:
Once you choose the memory category, you can narrow them down by various attributes: by nominal supply voltage, memory organization, maximum access time, memory density and temperature grade, to name a few. You will be able to find the right Combo Flash Memory, DRAM, Battery Backed SRAM, Dual Port Memory, EPROM, FIFO's, Flash Memory, EEPROM, Non Volatile SRAM, PSD Memory,FRAM, MRAM, Volatile Memory or Static RAM using these filters.
If the quantity of Memory devices you require is less than a full reel, we offer to our customers several of our programmable Memory devices in tray, tube or individual quantities that will help you avoid unneeded surplus.
Future Electronics also offers its clients a unique bonded inventory program designed to eliminate potential problems that may arise from an unpredictable supply of products that could contain raw metals and products with erratic or long lead times. Talk with your nearest Future Electronics branch and find out more on how you and your company can avoid possible shortages.