Montreal, Canada – Future Electronics, a global leading distributor of electronic components, is unleashing the true potential for wireless applications with the onsemi AXM0F343 System-on-Chip (SoC) in the latest edition of THE EDGE.
Included is the AX5043 radio is extremely powerful and is software programmable featuring the widest array of available modulation schemes, frequency range from 27 MHz to 1050 MHz, and data rates from 0.1 kbps to 125 kbps. Nearly any Sub GHz protocol, proprietary or standards based, can be implemented.
The onsemi AXM0F343 also contains the high performance ARM® Cortex®-M0+. Running at 40 MHz and between two variants, the high performance ARM® Cortex®-M0+ has either 64 kB of FLASH and 8 kB of RAM or 256 kB of FLASH and 32 kB RAM.
To learn more about the AXM0F343, visit www.futureelectronics.com/resources/featured-products/onsemi-axm0f343-system-on-chip-soc. To see the entire portfolio of products available through Future Electronics, visit www.FutureElectronics.com.
THE EDGE is the latest e-newsletter from Future Electronics, and is geared toward engineers and buyers looking for new or leading-edge products. THE EDGE comes out twice per month, and each edition features product information, datasheets and videos showcasing the most advanced new technology in a specific area, such as sensing, lighting, or automotive.
Visit www.FutureElectronics.com/subscribe to receive the latest issues of THE EDGE newsletter, and stay up to date with the newest technologies.