Future Electronics Corporate HQ Header Image

Future Electronics Highlights onsemi AR0830 Hyperlux™ LP Image Sensor for High-Performance, Low-Power Edge Vision Applications

Sign up to qualify for a FREE AR0830 Module compatible with the Future Electronics Goldilocks Platform, an NXP i.MX8M Plus demonstration system.

Montreal, Canada – Future Electronics, a leading global distributor of electronic components, is pleased to announce availability of the onsemi AR0830 Hyperlux™ LP Image Sensor, an 8.3 MP BSI Stacked CMOS sensor that combines high-resolution imaging with exceptionally low power consumption.

Part of onsemi’s cutting-edge Hyperlux™ LP family, the AR0830 sensor features a 1/2.9-inch form factor and a 3840 x 2160 active-pixel array, offering advanced imaging capabilities in both linear and enhanced dynamic range (eDR) modes through its rolling shutter readout. The sensor’s 1.4 μm BSI pixel enhances performance in low-light and near-infrared (NIR) conditions, delivering superior image quality for challenging edge environments.

The AR0830 is engineered with a robust feature set including:

  • Industry-leading low power consumption
  • Enhanced NIR response at 850nm and 940nm
  • Wake on Motion (WOM) functionality for efficient operation
  • Multiple subsampling modes including binning, summing, skipping, and windowing
  • Functional modes like Global Reset Release (GRR), trigger, and context switching
  • Advanced Line Interleaved HDR (LI-HDR) and eDR imaging modes

These capabilities make the AR0830 an ideal sensor for videoconferencing endpoints, video doorbells, AR/VR/XR headsets, machine vision, retail analytics, facial recognition systems, and wearables, among others.

onsemi’s Hyperlux LP family is tailored for applications where imaging quality, low latency, compact form factors, and energy efficiency are paramount. With a stacked architecture and proprietary technologies such as Smart ROI and optimized NIR sensitivity, Hyperlux sensors deliver high-resolution, high-fidelity images even in extreme lighting and environmental conditions.

For more information about the onsemi AR0830 Hyperlux™ LP Image Sensor and to sign up to qualify for a free AR0830 module, visit the dedicated Future Electronics landing page.

About Future Electronics

Founded in 1968, Future Electronics is a global leader in the electronic components industry. Future Electronics’ award-winning customer service, global supply chain programs and industry-leading engineering design services have made the company a strategic partner of choice.

Headquartered in Montreal, Canada, Future Electronics operates in 159 offices across 44 countries with over 5,000 employees. Its worldwide presence powers the company’s outstanding service and efficient, comprehensive global supply chain solutions. Future Electronics is globally integrated and supported by one IT infrastructure which provides real-time inventory availability and enables fully integrated operations, sales and marketing services worldwide. In 2024, Future became a WT Microelectronics company, now dual-headquartered in both Montreal, Canada and Taipei City, Taiwan.

Future Electronics’ mission is always to Delight the Customer®. For more information visit www.FutureElectronics.com.

Media Contact
Jamie Singerman
Corporate Vice President – Worldwide
FUTURE ELECTRONICS
www.FutureElectronics.com.
+1 514-694-7710
Jamie.Singerman@FutureElectronics.com