How to Engineer Automated Systems for Scalability, Cost, and Performance
What are the biggest differences and common mistakes when bringing a design from proof of concept to market?
Which hidden costs and technology choices make or break a successful, market-ready product?
And what are some key considerations teams should anticipate in order to scale reliably?
These were some of the questions we tackled during our latest Expert Panel. Read along for the insights, a detailed playbook, and a field-tested checklist for moving from demo to device.
Panelists

Bill Pratt
Regional Solutions Manager at Future Specialist Solutions

Cody Tudor
Analog/Power Specialist at Future Specialist Solutions

Serge Mvongo
Regional Sales Manager – Wireless and Sensors at Future Specialist Solutions

Laurent Helin
BDM – Embedded at Future Electronics’ Advanced Engineering Group

Lazina Rahman
IoT/Connectivity Specialist, Mediator
Why great prototypes fail
The industrial automation market is booming, and a single innovative idea can make waves in the industry.
But great ideas often meet tight deadlines. And while most engineering teams know the rush of putting together “quick and dirty” demos, fewer are able to completely avoid the stalls that follow: bringing that demo to a safe, manufacturable, and supportable product.
Bringing a design from proof of concept to production means:
- Ensuring reliability under varying circumstances.
- Safety compliance across different markets and regulatory bodies.
- Comprehensive documentation and scalable manufacturability.
- Packing all of this under tight power, thermal, and cost envelopes.
And this last one is probably the most common enemy to great prototypes: Hidden cost traps.
A prototype may get away with software that isn’t hardened for real‑world noise and latency. A marketable product will not. And adapting to that after may prove costly.
Same applies to motors, cables, and other mechanical components which inevitably wear out. And while a prototype may only need to survive long enough for a demo, a product is expected to provide long-term reliability. Selecting rugged materials for the long run may increase costs dramatically if not considered in early stages.
Is there a chance your product may be used for outdoor applications or harsh environments?
Then you must consider environmental ratings and the time and expense of concerning certifications (FCC/CE/UL/IEC, functional safety) as well as proper field testing.
All of these costs add up, and if not considered early, they may turn a good idea into a nightmare scenario.
How to approach this
Design for Manufacturing (DFM) early.
Forgotten subsystems tacked on after to pass a demo can explode costs later.
A bulletproof Design for Manufacturing considers assembly access, replacement order after parts A/B/C, and human/robot assembly time from the start.
Remember non‑technical assemblers will have to build thousands of these.
Supply chain longevity.
Choose sensors and compute parts that will still be available in 7–10 years; nothing derails a launch faster than an unexpected EOL on a critical component. Anchoring prototypes to production‑aligned KPIs helps prevent painful rework.
Platform strategy: Fast prototypes and smart pivots
Established commercial AI compute stacks offer great performance for prototyping, rapid algorithm validation, rich tooling, and a familiar developer experience that can greatly improve workflows in the lab.
But at scale, teams run into cost, power/thermal constraints (especially in enclosed robots), form‑factor limits (SOM + carrier), OTA friction, and EMI challenges around high‑speed GPU memory.
This is where NXP’s Ara-2 comes in.
For many production programs, pairing NXP processors with the Ara‑2 AI accelerator is a powerful solution to many of these issues.
This approach provides lower power operation, deterministic control options (via NXP i.MX or S32 families with FuSa pathways), acceleration that’s friendly to CNNs and transformers, and a Yocto‑based stack that are simpler to field‑maintain long‑term.
In addition, NXP’s eIQ toolchain helps keep ML workflows consistent from MCUs to MPUs, enabling tiered product lines.
Featured Product:

Explore the features of NXP’s Ara-2 Discrete Neural Processing Units
Learn more: i.MX 8M Plus Applications Processor | i.MX 8 Applications Processors
Where dedicated edge acceleration pays off
High‑intensity edge inference is where Ara‑2 excels, especially in scenarios that demand strong performance under tight power and cost constraints. Key strengths include:
- Computer vision workloads
- Object detection
- Object tracking
- Image and video classification
- Advanced model support
- Vision transformers (ViTs)
- Multimodal inference pipelines
- Operational advantages
- Efficient processing of parallel camera streams
- Low‑latency on-device decision‑making
- Built‑in privacy protections by keeping data local
These capabilities make Ara‑2 particularly compelling for smart‑city deployments, industrial automation, and any edge environment requiring real‑time, privacy‑sensitive visual intelligence.
Choosing motor control
Not all motor control components are made equal. Every motor category serves a different purpose, and choosing the right tool for the job can make a huge difference when it comes to size, power, architecture, and overall costs.
Stepper motors:
Stepper motors offer excellent precision and straightforward command via dedicated stepper drivers.
They require holding current to resist back‑driving, so they draw power even at rest. This makes them suitable for applications where accuracy is paramount and power budget allows.
Brushless DC (BLDC) (permanent‑magnet) motors:
BLDC motors deliver high torque/speed and power density. These are the go‑to for applications that require traction and moving mass.
However, they need three‑phase power stages and often require position sensing for precision.
High current/voltage implies heavier copper, thicker wires, and larger creepage/clearance on PCBs, impacting size and weight.
Additionally, its control algorithms and power electronics are more complex.
Brushed DC (BDC) motors:
BDC motors feature the lowest cost among the three and are the simplest to drive (e.g., H‑bridge).
This, of course, comes with trade-offs. BDC motors are far less efficient and precise, they wear out faster, and are often more power‑hungry than alternative options.
There are many applications, however, where they are still the right choice. Simple, non-critical motions like raising a status flag, for example, or powering a small propeller. Tasks where precision and speed are modest.
Explore: Future Technology Magazine Motor Control Articles
Takeaway:
Choosing the right motor control components is, as with most electronic design choices, a matter of what you want vs what you need.
Forcing low-cost BDC to do precision work with software gymnastics might result in added spending when it’s time to tackle complexity and tuning issues at a later stage.
Choosing a fancy BLDC motor to propel a miniature fan, on the other hand, might be overkill.
So when the time comes, take a step back and evaluate whether a stepper or small BLDC is the right architectural choice for the job at hand.
Sensors, fusion, and the compute/memory ripple effect
Sensors are the eyes and ears of an automated system. But it’s not just about having a clearer “vision”. You must also ensure the input data is communicated correctly and efficiently.
“Cheaper” sensors are often noisier, pushing you toward heavier filtering and sensor‑fusion strategies that increase compute and memory, ultimately affecting BOM and time‑to‑market.
It’s important to define your fusion level early (raw‑level vs feature‑level) and align with the compute, memory, and validation teams.
Equally important: confirm camera sensor ↔ ISP compatibility before you commit.
Choose the processor first, verify support lists second, and then pick the sensor that is right for the job.
Memory strategy
For modern inference, especially spatial models and transformers, memory bandwidth is the throttle.
While DDR3 can still serve small time‑series or RNN/LSTM tasks where latency isn’t critical, most edge AI designs lean toward DDR4/LPDDR4X → LPDDR5/LPDDR5X.
Data centers may even lean toward HBM3 → HBM3E to cut “time‑to‑first‑token” delays.
Depending on the case, memory and power must be treated as horizontal concerns across teams, not stovepipes on the compute side.
For certain robot classes, a capable MCU with DSP and on‑chip memory can avoid external DDR altogether, trimming cost and complexity.
When it comes to hybrid systems (e.g., i.MX + Ara‑2), evaluate if the accelerator’s internal buffering and pipelines cover the workload before adding DRAM.
And then comes the question of availability. DDR3 and DDR4 may come with limitations, but they are widely available and can get certain jobs done just as efficiently. Consider this when it’s time to choose, asking the question again, of what you want vs what you need.
A field‑tested checklist for moving from demo to device
- Lock safety & compliance early: threat models, functional safety plan, and a certification path (FCC/CE/UL/IEC).
- Budget field testing up front.
- DFM from day one: assembly access, replacement order, takt‑time for human/robot assembly, and error‑proofing.
- Avoid late “bolt‑on” subsystems.
- Choose production‑ready platforms
- Right‑size motors: map motion requirements to stepper / BLDC / BDC capabilities, and account for power electronics, wiring, and control complexity.
- Sensor/ISP due diligence: confirm compatibility lists before board spins; define fusion level with compute, memory, and test owners.
- Treat memory as a system resource: bandwidth governs inference; pick the lowest tier that meets accuracy + latency targets.
Get Expert Support
Design for the automated systems of the future.
Contact our engineers for expert guidance from start to finish.