Pays de livraison
Livraison gratuite aux États-Unis continentaux à partir de 50 $ US. Des conditions s'appliquent
Pays sélectionné
Un condensateur en aluminium électrolytique dispose d’une anode qui consiste en une fine feuille d’aluminium avec une surface gravée couverte d’oxyde d’aluminium qui agit en tant que diélectrique. Communément appelés e-caps, ils offrent les plus grandes valeurs de capacité par unité volumétrique par rapport aux condensateurs en céramique ou à film plastique. Future Electronics propose des condensateurs en aluminium électrolytique disponibles dans diverses capacités, impédances et cotes RSE. Nous disposons de condensateur à sorties perpendiculaires et de condensateur à sorties axiales, entre autres types.
Les condensateurs électrolytiques en aluminium montés en surface ...
Ajoutez de l’efficacité aux tests de circuits complexes grâce aux...
KYOCERA AVX features a range of aluminum capacitors called the AE...
A capacitor is a passive electrical component with two or more terminals which is used in order to store energy in an electric field. Capacitors contain at least two electrical conductors which are separated by a dielectric. When there is a voltage difference across the conductors, a static electric field develops across the dielectric, thus causing negative charge to collect on one plate and positive charge on the other. Energy is accumulated in the electrostatic field. Capacitance, measured in farads, is the ratio of the electric charge on each conductor to the voltage difference between them. Types of Aluminum Capacitors.
There are several different kinds of Aluminum Electrolytic capacitors at Future Electronics. Aluminum Electrolytic Capacitors, Aluminum Polymer Capacitors Super Capacitors, in many types. Axial, Radial, Surface Mount (SMD), Snap-in, Screw-Terminal, Hybrid Aluminum Polymer, Organic Polymer, Molded Polymer, Solid Polymer, Super Capacitors, Coin Type, Flat Type, Molded
We stock many of the most common types categorized by several parameters including capacitance, rated voltage, operating temperature range, case size / dimension, packaging type, usefull Life and several other attributes specific to each type of capacitor. Our parametric filters will allow you to refine your search results according to the required specifications.
Future Electronics has a wide range of aluminum capacitors from several manufacturers. Once you decide if you need Aluminum Electrolytic Capacitors, Aluminum Polymer Capacitors, you will be able to choose from their technical attributes and your search results will be narrowed to match your specific capacitor application needs.
We deal with several manufacturers such as Aishi, AVX, Cornell Dubilier, Eaton (Bussman) Elna, Epcos, Illinois Capacitor, Murata, Nic Components, Nichicon, Panasonic, Rubycon, Samwha, Surge, Taiyo Yuden, United Chemi-con, Vishay Wurth and Yageo America Corporation, among others. You can easily refine your capacitor product search results by clicking your preferred capacitor brand from the list of manufacturers below.
Capacitors have several uses in electrical and electronic systems. They are so widely used that it is rare that an electrical product does not contain some type of capacitor. Used mainly in bringing power to your device, is some cases a capacitor can store electric energy when it is disconnected from its charging circuit, so it can therefore be used like a temporary battery. They are often used in electronic devices in order to maintain a power supply while batteries are being changed thus preventing loss of information in volatile memory applications. In car audio systems, large capacitors are used to store energy for the amplifier to use when required. An uninterruptible power supply may be equipped with maintenance-free capacitors in order to extend its service life.
With the FutureElectronics.com parametric search, when looking for the right Aluminum Electrolytic capacitors, you can filter the results by category. We carry the following categories of capacitors:
Once you choose the capacitor category, you can narrow them down by various attributes: by capacitance, operating temperature range, rated voltage and case size / dimension, to name a few. You will be able to find the right Aluminum Polymer Capacitors, Aluminum Electrolytic Capacitors, by using these filters.
If the quantity of capacitors you require is less than a full reel, we offer to our customers several of our capacitors in tray, tube or individual quantities that will help you avoid unneeded surplus.
Future Electronics also offers its clients a unique bonded inventory program designed to eliminate potential problems that may arise from an unpredictable supply of products that could contain raw metals and products with erratic or long lead times. Talk with your nearest Future Electronics branch and find out more on how you and your company can avoid possible shortages.