Newly-introduced Renesas RA6M5 microcontrollers (MCUs) in the RA6 series featuring...
Read MoreFTM / AI, Security & Encryption / Microchip — DesignShield Security Protection Tool
Microchip has extended the security protection for the PolarFire® family of FPGAs with the DesignShield development tool, which helps to prevent Critical Program Information (CPI) from being extracted from FPGAs for malicious purposes.
The threats to mission-critical and other high-assurance systems deployed worldwide from cybercriminals are rapidly evolving. Manufacturers of these systems are looking for the strongest possible protection for CPI assets stored on the FPGAs which power them.
The new DesignShield tool from Microchip raises the barriers against cyber-attacks and reduces the risk of cloning, intellectual property theft, reverse engineering, or the insertion of malicious Trojan Horses. By deploying DesignShield on a PolarFire FPGA or the PolarFire SoC, a device manufacturer can ensure that deployed systems behave as intended, and are safe from counterfeiters and their threat to a developer’s design investments and brand reputation.
The DesignShield tool protects aerospace, defense, and other high-assurance systems from cybercriminals who try to acquire an FPGA’s bitstream from a system deployed in the field.
The tool deters reverse-engineering of the bitstream, which can often include CPI, by obscuring its logical equivalent using a combination of logic- and routing-based encryption techniques. This improves design security and integrity while reducing the risk of system corruption. It also lessens the chance that custom code, intellectual property, or information critical to national security are used by non-authorized agents.
The DesignShield tool is part of Microchip’s Libero development tool suite.
Based on non-volatile Flash memory, Microchip FPGAs offer inherently better security than SRAM-based alternatives which expose sensitive bitstream data on every power cycle.
Microchip FPGAs also include unique integrated security features which:
This layered approach to security includes licensed, patented differential power analysis protection, built-in certified security functions, built-in tamper detectors, and supply-chain assurance that the FPGA is authentic. With the DesignShield tool, Microchip has added another layer which protects the authenticity, integrity, and confidentiality of a design.
Share This
Get access to the latest product information, technical analysis, design notes and more
Newly-introduced Renesas RA6M5 microcontrollers (MCUs) in the RA6 series featuring...
Read MoreSusumu KRL Series low-resistance current-sensing chip resistors combine small package...
Read MoreRECOM RPX-4.0 Series Buck Converter Modules feature high power density...
Read MoreBe at the forefront of New Technology Innovations
Be at the forefront of New Technology Innovations
© 2025 Future Electronics. All rights reserved. Privacy | Terms & Conditions of Sale | Terms of Use | Accessibility