Making green energy a reality: How new electronic component technology supports the growth of the global hydrogen industry

January 9, 2025

By Steve Albuquerque Asia Region Business Development Manager for Energy Innovation, Future Electronics

As the world responds to the threat of climate change, hydrogen is emerging as a viable green energy source, both to complement batteries for zero-emission driving, and also as an energy storage medium.

 

Battery powered technology has been absorbing much of the available investment finance, to enable a shift to products such as electric vehicles and heat pumps which are not directly powered by fossil fuels. But as many countries work towards the achievement of ambitious net zero emissions targets for 2050, the development of green hydrogen power systems and hydrogen fuel supplies is also gathering momentum. This reflects the lack of constraint on the use of hydrogen, the most abundant element available for human use.

 

The majority of hydrogen produced today is made by splitting carbon from methane, but that produces carbon emissions. Zero-emission ‘green hydrogen’ comes from electrolysis, using clean electricity, from wind, solar or hydro sources, to split water into hydrogen and oxygen. Unlike batteries, which are unable to store large quantities of electricity for an extended period, hydrogen can be stored in large amounts for a long time. This makes it an ideal green storage solution for excess renewable energy.

 

Hydrogen has flexible uses: it can catalyze with oxygen to produce heat, or be fed into a fuel cell to make electricity. In a fuel cell, hydrogen has the potential to provide clean power for domestic use, as well manufacturing, transportation, and more. Hydrogen fuel can also complement wind and solar energy generation, providing a green energy storage solution to balance the intermittency of the renewable sources.

 

Industry watchers are now forecasting strong growth in the hydrogen industry. The Hydrogen Insights 2024 report, published by the Hydrogen Council, shows that the global hydrogen project pipeline grew by a factor of seven between 2020 and May 2024, from 228 projects to 1,572 projects [1]. Investment committed to projects at the final investment decision stage also grew from around $10bn across 102 projects in 2020 to $75bn across 434 projects in 2024.

 

China has stated the aim of having 50,000 hydrogen-powered vehicles on the road by 2025, while the European Union aims to produce 10 million tonnes of green hydrogen, powered by renewable energy sources, by 2030.

 

This growth in the hydrogen market is attracting companies to the commercial opportunities in the manufacturing, installation and operation of electrolysis plants. For green hydrogen, which is a zero-carbon fuel, this opportunity is particularly appealing in parts of the world with access to abundant sources of solar, hydropower or wind energy.

 

Electrolysis is a chemical operation, but it requires large amounts of electric power, either drawn from the grid or directly from wind turbines in so-called ac-dc coupled power systems, or directly from solar farms and battery storage in dc-dc coupled systems. The high-voltage power conversion equipment required to deliver the correct input to large electrolysis plants consuming megawatts of power has traditionally been the domain of a few global giant manufacturers such as ABB, Siemens and Schneider Electric. The growth in demand for electrolysis plants is opening up opportunities not only for these incumbents but also for smaller companies which have expertise in high-voltage power equipment manufacturing.

 

In the high-voltage equipment market, established and new suppliers will be judged by customers, the hydrolysis plant operators, on four crucial criteria:

  • Power quality
  • Efficiency
  • Reliability
  • Cost

 

This creates an opening for electronic component manufacturers to advance their position by providing products which help equipment manufacturers to improve products on any one or more of these criteria. This is leading to a new wave of innovation at component level.

 

Drive to improve efficiency and lower cost of hydrolysis

The basic process of hydrolysis is the same, whether it is implemented in a small-scale local production facility, such as a roadside hydrogen refueling station consuming less than 500 kW, or a bulk hydrogen manufacturing plant potentially consuming 20 MW or more. A single electrolysis cell, which separates water into hydrogen and oxygen, operates at a forward voltage of around 1.8 V to 1.9 V, depending on the temperature and the chemical additives used to enhance the electrolyte.

 

Current densities in the electrolyte range up to 0.5 A/cm². A direct current of 1,000 A can drive a cell with an area of 2,000 cm², generating roughly 1 kg of gaseous hydrogen per day [2].

 

Given that this basic chemical process has been well understood for many years, where is the scope to achieve future cost reductions and efficiency improvements? Currently, the cost of hydrogen produced via electrolysis ranges from $4 to $7 per kilogram, depending on the electricity price and electrolyzer efficiency. The US Department of Energy (DoE) has set a goal for this cost to fall to $2 per kilogram by 2025, and $1 per kilogram by 2030.

 

Achieving these cost reduction targets will require substantial improvements in electrolyzer efficiency as well as improved economies of scale resulting from the large-scale deployment of electrolysis plants.

 

Some of the efficiency gains for electrolysis plants will have to come from more efficient power conversion systems. And this is sharpening the industry’s focus on the improved component offerings from the main suppliers to high-voltage equipment manufacturers, such as Infineon and Littelfuse.

 

Ac-dc coupled systems: battle between thyristors and IGBT switches

For instance, in ac-dc coupled power systems, electrolysis plants adopt a range of configurations of the power conversion system, shown in Figure 1), typically based on either a diode/thyristor rectifier topology, or an IGBT-based active front end (AFE) topology. AFE rectifiers can be operated at unity power factor, and produce total harmonic distortion (THD) of less than 5%.

Future Electronics — Growth of the Global Hydrogen Industry

Fig. 1: Typical hydrolyser plant configurations in ac-dc coupled settings. (Image credit: Infineon)

For decades, the dominant topology in ac-dc coupled electrolysis has been the thyristor-based 12- or 24-pulse system, shown in Figure 2. The main benefits of these architectures are robustness, high efficiency levels, and high current density. Thyristor rectifiers are particularly useful in high-power applications consuming more than 1 MW. Even high system power configurations operating at more 50 MW can be efficiently implemented with an array of high-power thyristors and diode discs.

 

Thyristor-based designs have been in operation in the field for decades, and the press-pack devices used in them offer superior power and thermal attributes.

Future Electronics — Growth of the Global Hydrogen Industry

Fig. 2: A thyristor-controlled B12C rectifier driven by a dedicated transformer. (Image credit: Littelfuse)

In some industrial electrolyzers, the current flowing through the rectifier can be in a range between 1.5 kA and 2.0 kA. For such high-power systems, both Littelfuse and Infineon offer integrated power solutions called power stacks, power blocks and power discs. Littelfuse offers the N1718NC200 phase-controlled thyristor capsule for up to 2.0 kA applications.

 

For high-voltage electrolyzers, Infineon supplies a component choice for any choice of topology. This includes AFE rectifiers, which can use its TRENCHSTOP™ 7 IGBT technology and/or CoolSiC™ silicon carbide (SiC) MOSFETs at lower power levels up to 100 kW, and IGBT-based PrimePACK™ modules at up to 5 MW.

 

Thyristor vs IGBT: the pros and cons

Efficiency: IGBT systems offer higher energy efficiency than thyristor rectifiers. In green hydrogen electrolysis, in which it is important to maximize efficiency, IGBTs can minimize energy loss during power conversion.

Current and voltage handling: thyristor rectifiers are more suitable for large-scale hydrogen electrolysis plants as they can handle higher currents and voltages. Although IGBTs are efficient, thyristors excel at managing high power levels, making them ideal for extensive hydrogen production systems.

Control and precision: IGBTs provide more power control and precision than thyristors. IGBT systems also provide greater flexibility in the control of voltage and current, ensuring the smooth and efficient operation of hydrogen electrolysis equipment.

Installation and maintenance: IGBT systems are typically smaller and easier to install than thyristor rectifiers. However, thyristors offer excellent durability and require less maintenance, making them a cost-effective option for large-scale industrial hydrogen production plants.

 

Both IGBT-based and thyristor rectifier-based topologies play a role in optimizing the efficiency and performance of green hydrogen electrolysis systems. Understanding the advantages of each technology can help the manufacturer to choose the correct option for hydrogen production requirements.

 

Dc-dc coupled systems: wide bandgap innovation

In dc-dc coupled systems powered by solar energy and/or batteries, typical topologies used for power conversion in hydrolysers are:

  • Interleaved buck
  • Dual active bridge, shown in Figure 3
Future Electronics — Growth of the Global Hydrogen Industry

Fig. 3: Topologies for conversion in hydrolyser dc-dc coupled conversion systems. (Image credit: Infineon)

Here too, component innovation is helping to power equipment manufacturers to meet the market need for higher efficiency and reliability at lower system cost. For instance, Infineon is enabling manufacturers to take advantage of the superior electrical and thermal attributes of SiC MOSFETs with a new CoolSiC FET series which offers a breakdown voltage rating of up to 2,000 V.

 

Supplied in an HCC package with 14 mm creepage and 5.5 mm clearance distances, the IMYH200RxxxM1H MOSFETs are available with on-resistance as low as 12 mΩ. Use of these MOSFETs in electrolysis gives benefits including:

  • Low conduction and switching losses
  • Low reverse-recovery loss
  • Excellent thermal performance
  • Robust body diode for hard commutation

While these discrete devices are suitable for electrolyzers operating at 10 kW to 100 kW, integrated modules are available for use in higher-power applications of 1 MW and more. Infineon has extended the capability of its PrimePACK 3+ modules with the latest IGBT7 family, which has devices with a high 2,300 V breakdown voltage rating.

 

The IGBT7 devices are rated for over-temperature operation, and provide very high current density in their 247 mm x 89 mm x 38 mm form factor. For instance, the FF2400R12IP7 PrimePACK module supports currents up to 2.4 kA and voltages up to 1,200 V in an interleaved buck converter.

 

In the dual active bridge topology, Infineon solutions include the FF2000XTR33T2M1 SiC MOSFET module in an XHP package, supporting 3.3 kV operation and featuring on-resistance of just 2 mΩ, while the FF1800R23IE7 IGBT7 module provides 2.3 kV/1.8 kA ratings.

 

Innovation in power components contributes to growth in hydrogen market

The aggressive hydrogen cost-reduction targets set by the US DoE reflect the role of hydrogen production as a key enabling technology for the adoption of hydrogen and fuel cell technologies in applications including stationary power, portable power, and transportation.

 

The achievement of the 1:1:1 target, of $1 for 1kg of hydrogen in one decade, will depend on advances in technology throughout the hydrolyser process, as well as expanding deployments to produce economies of scale.

 

Continual improvements in power component efficiency, and the widening range of product and package options, will give the manufacturers of power equipment for electrolysis plants greater scope to create value and enable the growth in this new fuel type to accelerate.

Related Articles

Renesas — RA0 Series Microcontrollers
Power your innovations with Renesas' RA0 series microcontrollers. Discover their performance and eff...
Read More
American Zettler — AZSR170 70A Solar Power Relay
Relays with wide contact gap switch up to 70 A/600 V Facebook Linkedin-in Youtube The...
Read More
Vishay — SE20ND Surface-Mount Standard Rectifier
New low-profile rectifier IC offers footprint compatibility with legacy packages Facebook Linkedin-in Youtube The...
Read More

Subscribe to our newsletters

Subscribe to Future Electronics

Get access to the latest product information, technical analysis, design notes and more

Choose your region