Shipping Country
Free shipping within the continental US over $50. Conditions apply
Select Country
Manufacturer Part #
1241380-2
Download the CAD models for this product. Learn more about SnapMagic.
4500 per Reel
Shipping Information:
HTS Code:
ECCN:
PCN Information:
General Product Description:PCN_A_01_OthersDescription:This product Change Notification (PCN) is to inform about a tool transfer, from TE Speyer to TE Dinkelsbuehl, according to VDA trigger matrix no. 29 and AIAG section 3.1 item 4. The change has no impact to form-fit-function.TE Change process follows a strict procedure, which fully maintains quality and ability to supply. Internal release process is ensured by TE, including product validation as per OEM/CAM requirements (when applicable). Validation will be initiated and completed according to project plan, as soon as samples are available.Reason for Changes:As a result of a thorough analysis of demand picture, matching our customer needs, we are going to optimize value stream of PNs in scope of this PCN. This change will support the need of our customers for shorter lead-times and optimized value streams.First Date To Ship (Changed Parts Only): 30-JAN-2026
General Product Description:PCN_A_01_OthersType of Change Manufacturing Location ChangeDescription of ChangesThis product Change Notification (PCN) is to inform about a tool transfer, from a TE Speyer to TE Dinkelsbuehl, according to VDA trigger matrix no. 29 and AIAG section 3.1 item 4. The change has no impact to form-fit-function. TE Change process follows a strict procedure, which fully maintains quality and ability to supply. Internal release process is ensured by TE, including product validation as per OEM/CAM requirements (when applicable). Validation will be initiated and completed according to project plan, as soon as samples are available. PPAP will be prepared (as per agreements between the two parties, including the negotiated TE trigger matrix), a request via ePPAP (via www.te.com or request to TE Sales representative) needs to be initiated by Customer 4 weeks prior to implementation date. In case no request is obtained till above mentioned date, PPAP will be considered as approved, and the change is considered as fully releasedReason for Changes:As a result of a thorough analysis of demand picture, matching our customer needs, we are going to optimize value stream of PNs in scope of this PCN. This transfer will support the need of our customers for shorter lead-times and optimized value streamsFirst Date To Ship (Changed Parts Only):26-JAN-2026
General Product Description:PCN_A_01_OthersDescription of ChangesThis product Change Notification (PCN) is to inform about a tool transfer, from a TE Speyer to TE Dinkelsbuehl, according to VDA trigger matrix no. 29 and AIAG section 3.1 item 4. The change has no impact to form-fit-function. TE Change process follows a strict procedure, which fully maintains quality and ability to supply. Internal release process is ensured by TE, including product validation as per OEM/CAM requirements (when applicable). Validation will be initiated and completed according to project plan, as soon as samples are available. PPAP will be prepared (as per agreements between the two parties, including the negotiated TE trigger matrix), a request via ePPAP(via www.te.com or request to TE Sales representative) needs to be initiated by Customer 4 weeks prior to implementation date. Incase no request is obtained till above mentioned date, PPAP will be considered as approved, and the change is considered as fully released.Reason for Changes:Product improvement.As a result of a thorough analysis of demand picture, matching our customer needs, we are going to optimize value stream of PNs in scope of this PCN. This change will support the need of our customers for shorter lead-times and optimized value streams.First Date To Ship (Changed Parts Only):20-MAY-2026
Description of ChangesDear customer, we would like to inform you about new coding 1241380-2 and 1564324-2 add on mass production tool 11-1209324 in China TE Suzhou plant for production to support only Asia-Pacific market. EMEA customer do not need to change the China part, only keep original EMEA part.Reason for Changes:Customer Request. Customer request, as a result of our continuous strive for capacity increase of our production, we hereby inform you upfront about new coding 1241380-2 and 1564324-2 add on mass production tool 11-1209324 in China TE Suzhou plant, which is under construction in order to meet all specification requirements to cover increasing marked demand and which will run in addition to current one. EMEA customer do not need to change the China part, only keep original EMEA part.
Description of Changes:The Suzhou factory in China will replace the following series of part numbers' outer carton. Compared with the old version of the outer box, the size of the new outer box is consistent with the original outer box, only the material and model of the outer box are changed, which does not affect the product itself. Meanwhile, the new carton has passed the drop test of TE, which is in line with the product packaging specifications of TE, it can ensure product safety.Reason for Changes:Customer Request. Dear customer, we hereby inform you that the part number in the following attachment will be changed to a new outer box. The size of the new outer box is the same as the old one, only the material and model are changed. At the same time, the new carton has passed TE's drop test and conforms to TE's product packaging specifications to ensure the safety of terminals in the carton. This change does not involve the change of the product itself, but only changes the outer packaging box of the product, which does not affect the product.
Part Status:
Inventory held at our manufacturer's warehouse. Subject to availability and transit time.