Shipping Country
Free shipping within the continental US over $50. Conditions apply
Select Country
Manufacturer Part #
SI4401FDY-T1-GE3
Download the CAD models for this product. Learn more about SnapMagic.
2500 per Reel
SOIC-8
Surface Mount
Shipping Information:
HTS Code:
ECCN:
PCN Information:
Description of Change: Vishay Siliconix announces the B/E site-transfer from Vishay Simconix to the new subcontractor, ATEC (AutomatedTechnology (Phil.) Inc.), as the capacity expansion of assembly and testing for Commercial Low-Voltage Power MOSFET in SO-8 Single and Dualpackages. ATEC locates in Laguna, Philippines, and professionally engages in assembly and test of power semiconductor devices with the major certificates,including ISO-14001, ISO-9001, IATF-16949, and VDA6.3 compliant.Reason for Change: Capacity ExpansionStart Shipment Date: Wednesday September 30, 202
Description:No Physical, Process, or Location Changes We want to emphasize that products continue to be manufactured at the same locations, using the same equipment, materials, packaging, and process steps as before. There have been no changes to any aspect of the production process or sites involved.BackgroundThis alignment is part of a global initiative at Vishay to ensure consistent representation of CoO information across all divisions, based on international and national regulations, as well as World Trade Organization guidelines.Please NoteSome customers may have already noticed changes in the CoO information on documentation accompanying recent product deliveries. As part of this ongoing initiative, updates to the CoO may continue to appear over time in product documentation, where applicable. These changes align with the updated approach and do not reflect any physical changes to the products themselves.
Description of Change: To meet the increasing demand for commercial Power MOSFET products, Vishay Siliconix announces the qualification of wafer BGBM process (Backside-Grind and Backside-Metallization) for commercial Low-Voltage Power MOSFETs at in-house Siliconix Philippines Inc.(SPI) facility in Binan, Philippines.Reason for Change: Capacity Expansion
Description of Change: Due to the fire accident in Jan-2023, the original plating subcon of Vishay Siliconix, Welnew-Wuxi, is suspended and will be entirely replaced by the new site in Shanghai, China (Welnew-Shanghai). This full release of Welnew-Shnaghai applies to commercial product packages with copper lead-frame assembled in Simconix in Shanghai. Welnew-Shanghai was founded in 2006 as a leading provider of Hall sensor products, semiconductor process service, and equipments. Welnew-Shanghai has achieved the certifications, including IATF-16949, ISO-9001, and ISO-14001.Expected Influence on Quality/Reliability/Performance: There will be no effect on quality, reliability, performance, and the minimum/maximum values in the datasheet.Time Schedule:Start Shipment Date: Wed Jul 5, 2023
Part Status:
Inventory held at our manufacturer's warehouse. Subject to availability and transit time.