Shipping Country
Free shipping within the continental US over $50. Conditions apply
Select Country
Manufacturer Part #
515-1061-801F
Download the CAD models for this product. Learn more about SnapMagic.
100 per Bag
Shipping Information:
HTS Code:
ECCN:
PCN Information:
REVISION:Pls find the attached file to revise the plant move date for the Dialight Penang, MYS location. 1/12/2024: Revised test on cover sheet Added additional page listing affected part numbers4/18/2024: Updated key dates Based on revised information from MalaysiaNEW ADDRESS:Dialight Penang Sdn Bhd No.1478B,Lorong Perusahaan Maju 8, Kawasan Perusahaan Perai, 13600 Perai,Pulau Pinang, Malaysia.Change Description:Moving the existing facility in Penang, Malaysia to a new facility in Penang, Malaysia 2 blocks (150 m) away. There will be no change to current BOMs, standard operating procedures, staffing or equipment. New building configuration will allow for all production lines to be moved to the mew facilities and maintain the exact layout of production lines as the current building. The new site will be fully qualified by Dialight Operations, Engineering and Quality teams. Reason:Lease on existing building expiring. Move to new facility 2 blocks (150m) away required to provide improved efficiencies and capacity utilization to better support Dialight component's customers demands.
Change Description:Moving the existing facility in Penang, Malaysia to a new facility in Penang, Malaysia 2 blocks (150 m) away. There will be no change to current BOMs, standard operating procedures, staffing or equipment. New building configuration will allow for all production lines to be moved to the mew facilities and maintain the exact layout of production lines as the current building. The new site will be fully qualified by Dialight Operations, Engineering and Quality teams.Reason:Lease on existing building expiring. Move to new facility 2 blocks (150m) away required to provide improved efficiencies and capacity utilization to better support Dialight component's customers demands.The new address for the new MYS plant is as below : Dialight Penang Sdn Bhd No.1478B,Lorong Perusahaan Maju 8, Kawasan Perusahaan Perai, 13600 Perai,Pulau Pinang, Malaysia. The move will take place end of March into April of 2024.
Part Status:
The 515-1061-801F is a 3 mm round optopipe optical light pipe.
This Optopipe is held in place by 2 press-fit pins along the bottom of the device. The light pipe is not attached to the panel at any point but can protrude through holes in the panel. The gently arcing emitting end sticks through the plastic or metal panel.
Features:
Inventory held at our manufacturer's warehouse. Subject to availability and transit time.