Shipping Country
Free shipping within the continental US over $50. Conditions apply
Select Country
Manufacturer Part #
5P49V5901B000NLGI
Download the CAD models for this product. Learn more about SnapMagic.
490 per Tray
VFQFPN-24
Surface Mount
Shipping Information:
COO is assigned at time of shipping and cannot be selected during the ordering process. All documents will indicate COO at time of shipping
HTS Code:
ECCN:
PCN Information:
Subject: Unisem Internal Manufacturing Transfer for QFN assembly facility from UNISEM SIMPANG PULAI (USP) to UNISEM GOPENG (UGP). Description of Change: This notice is to inform you that Unisem has officially announced the opening of its second state-of-the-art assembly and test facility, i.e. Unisem Gopeng (UGP) located in Gopeng, Perak.Unisem internal manufacturing transfer is necessary to align and optimize mass production in support of Unisem?s capacity expansion program. As of the date of this notice, Unisem?s internal manufacturing transfer as well as Renesas product and site-specific qualification activities at the UGP facility are complete. Renesas will begin using Unisem Gopeng (UGP) as an alternate site for assembly of the listed Renesas packaged products. Reason for Change: Internal manufacturing transfer is necessary to ensure continued product manufacturability in support of customer delivery requirements. Effective Date: 8/4/2026
Subject: Add Alternate Assembly Locations on Select VFQFPN PackagesDescription of Change:Renesas is adding JCET, China as an alternate Assembly location on select VFQFPN packages. The alternate assembly location is the current qualified location for Renesas. The material sets of the current and the alternate assembly locations are as shown in the below table. There will be changes in the material sets, equipment models and inspection items and sampling at the alternate location. The process flows are identical at all the qualified assembly locations.
This revised notice is to add additional part numbers to this change.Description of Change:Renesas is adding Unisem, Malaysia as an alternate assembly location for VFQFPN packages. Unisem has been qualified by Renesas as an approved Assembly location.Refer to below table for the current and the alternate assembly locations and its material sets by package type.There will be changes in the material sets at the alternate assembly location.Reason for Change:The change is for increased manufacturing capability and business continuity.No change in the moisture sensitive level as a result of this change.
Part Status:
Inventory held at our manufacturer's warehouse. Subject to availability and transit time.