Shipping Country
Free shipping within the continental US over $50. Conditions apply
Select Country
Manufacturer Part #
SI1922EDH-T1-GE3
Download the CAD models for this product. Learn more about SnapMagic.
3000 per Reel
SOT-363 (SC-70-6, SC-88)
Surface Mount
Shipping Information:
COO is assigned at time of shipping and cannot be selected during the ordering process. All documents will indicate COO at time of shipping
HTS Code:
ECCN:
PCN Information:
Description:No Physical, Process, or Location Changes We want to emphasize that products continue to be manufactured at the same locations, using the same equipment, materials, packaging, and process steps as before. There have been no changes to any aspect of the production process or sites involved.BackgroundThis alignment is part of a global initiative at Vishay to ensure consistent representation of CoO information across all divisions, based on international and national regulations, as well as World Trade Organization guidelines.Please NoteSome customers may have already noticed changes in the CoO information on documentation accompanying recent product deliveries. As part of this ongoing initiative, updates to the CoO may continue to appear over time in product documentation, where applicable. These changes align with the updated approach and do not reflect any physical changes to the products themselves.
Description of Change: To meet increasing demand with more flexibility for power MOSFETs, Vishay Siliconix announces the qualification of the new solder-plating site, Welnew-Shanghai, in Shanghai city, China. This full release of Welnew-Shnaghai applies to commercial product packages with copper lead-frame assembled in Simconix in Shanghai.Reason for Change: Manufacturing Capacity Expansion
Description of Change: .To meet increasing demand with more flexibility for power MOSFETs, Vishay Siliconix announces the qualification of the new solder-plating site, Welnew-Shanghai, in Shanghai city, China. This full release of Welnew-Shnaghai applies to commercial product packages with copper lead-frame assembled in Simconix in Shanghai.Welnew-Shanghai was founded in 2006 as a leading provider of Hall sensor products, semiconductor process service, and equipments.Welnew-Shanghai has achieved the certifications, including IATF-16949, ISO-9001, and ISO-14001.Reason for Change: Manufacturing Capacity Expansion
Part Status:
On Order
Inventory held at our manufacturer's warehouse. Subject to availability and transit time.