Manufacturer Part #
KLKD001.T
ELECTRICAL 1 AMP
| | |||||||||||
| | |||||||||||
| Mfr. Name: | Littelfuse | ||||||||||
| Standard Pkg: | Product Variant Information section Available PackagingPackage Qty:10 per Bag Package Style:CARTRIDGE Mounting Method:Surface Mount | ||||||||||
| Date Code: | |||||||||||
Littelfuse KLKD001.T - Product Specification
Shipping Information:
ECCN:
PCN Information:
**Update to FPCN107852**Description:This formal Part Change Notification (PCN) is for the change from the current UL Listed or cULus certification mark to the enhanced UL mark on our 0SPF, KLKD, SPXC, SPXV and SPFJ fuse product labels for Suzhou and Mexico-manufactured products. Existing CSA marks which are found only on Mexico-made components will be maintained. China-made versions (CN suffix) do not have CSA. There are NO CHANGES in the fit, form, and function of the fuses.Update Summary:Attached is the revision of LFPCN_PG0191. This is to notify the team on the change from the ?UL listed? and ?cULus? marks to the ?Enhanced UL mark? on the label of the following fuse series: 0SPF, KLKD, SPXV, SPXC (added in this revision), SPFJ (added in this revision). Please take note that existing CSA marks will remain unchanged. This is a running change from July to December 2024.
Subject: Replacing ?UL Listed? and ?CSA? or ?cULus? logos with enhanced UL mark on Fuse LabelThis formal Part Change Notification (PCN) is for the change from the current UL Listed, CSA, or cULus certificationmark to the enhanced UL mark on our 0SPF, KLKD, and SPXV fuse product labels for Suzhou and Mexicomanufacturedproducts. The are NO CHANGES in the fit, form, and function of the fuses.
Manufacturing location change:Dear Valued Customer, The purpose of this letter is to notify you about a manufacturing location change for the Industrial fuse products we currently supply to you. As we execute the Littelfuse growth strategy, we will relocate the manufacturing facility of the Industrial Circuit Protection Fuses to a new location in Piedras Negras, Coahuila, Mexico. This change is focused on a unified product line strategy to support all business units' expansion across the company. This project will be completed in Q1 2024. This facility will be relocated within the same city as our current factory, around 6.5 km apart from our current location.The new site will increase our footprint, improve our manufacturing capacity, and align our customer focus to provide a better response time. Our new address will be: Parque Industrial Piedras Negras Avenida Industrial y Libramiento Manuel Pere Trevi?o Interior #19 Piedras Negras, Coahuila, M?xico Zip Code 26070 Littelfuse has built a safety stock to ensure a smooth transition from one plant to another.
Part Status:
Littelfuse KLKD001.T - Technical Attributes
| Voltage Rating: | 600V |
| Rated Voltage (VAC): | 600VAC |
| Response Characteristic: | Fast-Acting |
| Current Rating: | 1A |
| Interrupting Rating: | 100kA |
| Dimension: | L 38.1mm x D 10.31mm |
| Package Style: | CARTRIDGE |
| Mounting Method: | Surface Mount |
Available Packaging
Package Qty:
10 per Bag
Package Style:
CARTRIDGE
Mounting Method:
Surface Mount