Manufacturer Part #
DF11-12DS-2C
DF11 Series 12 Position Dual Row 2 mm Pitch Crimp Socket
Hirose Electric DF11-12DS-2C - Product Specification
Shipping Information:
ECCN:
PCN Information:
Update!!!The previous official document 430-21018 notifying Toray Corporation of whether the UL certification was unqualified was confirmed as follows: 1. Announcement from Toray (1) For all applicable materials for which inappropriate acts were made in FUS (follow-up service) in the past, it has been decided that the existing UL certification registration is unchanged as it is.(2) Even for grades for which inappropriate acts were not made, UL certification registration is unchanged as it is. 2. Impact on HiroseAs UL certification registration of Amilan/TORAYCON is unchanged, there is no impact on UL certification registration of our products using Amilan/TORAYCON.We continue to supply our products using the applicable materials.
UPDATE to previous PCN 88110..Impact on our products by Inappropriate Identification on Nylon resin Amilan and PBT resin TORAYCON of Toray Industries, Inc. Toray Industries, Inc. (Hereinafter Toray) announced followings about Nylon resin Amilan and PBT resin TORAYCON (Hereafter Applicable materials) that were improperly identified as receiving certification from Underwriters Laboratories, a third-party safety science organization in the United States (hereinafter, "UL"). We are writing to inform you of the impact on our products. 1 Announcement from Toray As a result of discussions between UL and Toray regarding the handling of UL certified applicable materials, Toray received the following conclusion from UL. (1) For all applicable materials for which inappropriate actions were made in FUS (follow-up service) in the past, it has been decided that the existing UL certification registration continues as it is. (2) Even for grades for which inappropriate actions were not made, UL certification registration continues as it is. Impact on our products:From the announcement from Toray that the UL certification registration of the applicable materials continues, there is no impact on UL certification registration of our products using the applicable materials.
ChangesAdding new manufacturer for the resin in addition to current manufacturer.There is no change on product specifications and connector ULrecognition File No. (E52563)We will inform you again after we receive UL recognition for the resin made by another manufacturerReason for changeTo ensure resin supply stability.Timing of changeStart from Nov. 1sat 2022We applied for certification to UL for adding resin manufacturer under each connector series name.But The timing may change depending on UL recognition status, our inventory and our production stat.
It was previously notified that the following 14 items will be added to the new material housing, and the updated estimated production date.HIROSE would like to report on the addition of material manufacturers for DF3 series and DF11 series products.Action and ReasonTo improve and stabilize connector supply, we are going to add a housing material supplier for the above connectors.UL and CSA are already certified for those connectors with the additional material.(The connectors with the additional material are equivalent with the ones with the current material in terms of performance.)
HIROSE would like to report on the addition of material manufacturers for DF3 series and DF11 series products.Action and ReasonTo improve and stabilize connector supply, we are going to add a housing material supplier for the above connectors.UL and CSA are already certified for those connectors with the additional material.(The connectors with the additional material are equivalent with the ones with the current material in terms of performance.)
Part Status:
Hirose Electric DF11-12DS-2C - Technical Attributes
Type: | Crimp Contact |
No of Positions: | 12 |
Pitch: | 2 mm |
Style/Orientation: | Receptacle |
Termination: | Crimp |
Features & Applications
Available Packaging
Package Qty:
100 per Bag