Renesas — AE-CLOUD2 Kit | Futureelectronics NorthAmerica Site
text.skipToContent text.skipToNavigation

 

 

Renesas

 

The newly launched AE-CLOUD2 cloud connectivity kit quickly enables developers to create their next-generation IoT device using the latest cellular technology. With the AE-CLOUD2, developers can now choose between wired Ethernet, Wi-Fi, or CAT-M1/NB-IoT cellular technology to connect their device to the Internet and on to the cloud. AE-CLOUD2 provides maximum freedom in choosing how their device will connect.
 

Expand Your Device Reach with Global Cellular Connectivity

With the addition of an LTE CAT-M1 and NB-IoT cellular option for AE-CLOUD2, developers now have the flexibility to create devices that can be placed anywhere in the world where cellular coverage exists. Devices can now be truly mobile and wireless, enabling a whole new class of IoT devices. Low power, low data rates, and lower modem device costs are key for IoT and M2M devices to be successful. Unlike other LTE technologies, CAT-M1 and NB-IoT are specifically geared to tackle these device and market challenges. AE-CLOUD2 and Renesas Synergy support this with a packaged solution using CAT-M1 and NB-IoT out-of-the-box.
 

Create. Connect. Cloud.

Just like previous kits, AE-CLOUD2 quickly enables customers to connect to enterprise cloud service providers like Amazon Web Services, Google Cloud Platform, and Microsoft Azure, as well as connecting to a private cloud instance using Medium One. Developers can quickly demo and prototype on each platform to fi t their needs. Coupled with the different connectivity options, there is now a vast array of options to get your IoT device communicating with the cloud quickly and easily. Get started on your development path with application projects for each of the aforementioned cloud providers, or just kick the tires with a cloud demo so you can see what your IoT device can be capable of doing!
 


Synergy AE-CLOUD2 Development Kit

The AE-CLOUD2 kit comes out-of-the-box with Ethernet, Wi-Fi, and cellular RF transceivers. Simply get a SIM card and data plan, install the SIM card, load up either the cloud demo application or any of the free cloud application projects, and you are off and running toward your next connected IoT design. Use the AE-CLOUD2 and included cloud connectivity software to jumpstart your next IoT design today!


 

Renesas Synergy
FTM NA SideNav SubscribeTile EN
FTM NA NovDec2018 SideNav Download