Pays de livraison
Livraison gratuite aux États-Unis continentaux à partir de 50 $ US. Des conditions s'appliquent
Pays sélectionné
Un microcontrôleur 16-bit est un système intégré qui inclut de la mémoire, un processeur, et des périphériques qui peuvent facilement être intégrés à d’autres systèmes pour un fonctionnement fluide. Future Electronics propose un large éventail de microcontrôleurs génériques 16-bit. Nos microcontrôleurs 16-bit sont classés par tailles de flash, nombres de lignes d’entrée/sortie, types de packaging, volumes de RAM, tensions d’alimentation et vitesses. Explorez simplement la collection et trouvez celui qui convient le mieux à votre application.
The dsPIC33A family of DSCs by Microchip with low latency respons...
The i.MX 8M Plus family by NXP is designed to excel in machine le...
The dsPIC33AK128MC106 General Purpose DIM (EV02G02A) by Microchip...
Future Electronics & Renesas are proud to introduce the Maple Can...
A 16 bit microcontroller is a self-contained system with memory, peripherals and a processor that can be used as an embedded system. Most programmable 16 bit microcontrollers used today are embedded in other consumer products or machinery including telephones, automobiles, household appliances and peripherals for computer systems. Therefore, another name for a 16 bit microcontroller is "embedded 16 bit controller." Some embedded systems are more sophisticated whereas others have minimal requirements for memory and programming length with a low complexity for the software. Input and output devices include LCD displays, relays, solenoids, switches and sensors for data such as temperature, humidity or light level, amongst others.
There are many different kinds of programmable 16 bit microcontrollers. At Future Electronics, we stock many of the most common types categorized by several parameters including Flash size, number of input/output lines, packaging type, RAM size, supply voltage and speed. The parametric filters found on our website will allow you to refine your search results according to the required specifications.
The most common sizes for RAM are 1.5 kB, 2 kB, 4 kB, 8 kB, 16 kB, and 32 kB. We also carry 16 bit microcontrollers with RAM sizes up to 768 kB. Flash sizes can range from 4 kB to 1.5 MB, with the most common sizes being 16 kB, 32 kB, 64 kB, 128 kB, 256 kB and 512 kB.
Programmable microcontrollers contain general purpose input/output pins and the number of these pins may vary depending on the microcontroller. They can be configured by software to an input or output state. When these pins are configured to an input state, they can be used to read external signals or sensors. When they are configured to the output state, these pins can drive external devices like motors and LED displays.
Future Electronics has a full selection of programmable 16 bit microcontrollers, including low power, LCD, pic, wireless, and USB microcontrollers from several manufacturers. Simply choose from the 16 bit microcontroller technical attributes below and your search results will be narrowed to match your specific 16 bit microcontroller application needs.
We deal with several manufacturers. You can easily refine your programmable 16 bit microcontroller product search results by clicking your preferred 16 bit microcontroller brand from our list of manufacturers below.
Programmable 16 bit microcontrollers are designed to be used for embedded applications, contrary to microprocessors that can be found in PCs. 16 bit microcontrollers are used in automatically controlled devices including implantable medical devices, power tools, toys, office machines, engine control systems, remote controls, appliances as well as other types of embedded systems.
With the FutureElectronics.com parametric search, when you are looking for the right 16 bit microcontrollers, you can filter the results by various attributes: by RAM size (1.5 kB, 2 kB, 4 kB, 8 kB, 16 kB, 32 kB, …), Flash size (16 kB, 32 kB, 64 kB, 128 kB, 256 kB, 512 kB,…), number of input lines (from 2 to 119 lines), speed (16 MHz, 20 MHz, 32 MHz, 40 MHz, 50 MHz, 80 MHz,…) and supply voltage (up to 32V) to name a few. You will be able to find the right 16 bit low power, LCD, USB, pic or wireless microcontrollers using these filters.
If the quantity of 16 bit microcontrollers that is required is less than a full reel, we can offer customers several of our programmable 16 bit microcontrollers in tube, tray or individual quantities that will help you avoid unneeded surplus.
In addition, Future Electronics offers to clients a unique bonded inventory program that is designed to eliminate potential problems that can arise from an unpredictable supply of products that may contain raw metals and products with long or erratic lead times. Talk with your nearest Future Electronics branch and find out more on how you and your company can avoid possible shortages.