Pays de livraison
Livraison gratuite aux États-Unis continentaux à partir de 50 $ US. Des conditions s'appliquent
Pays sélectionné
Les commutateurs DIP sont des commutateurs compacts fournis dans des boîtiers à double rangée de connexions et pouvant être montés directement sur une carte de circuit. Future Electronics distribue des commutateurs DPDT, DPST, SPDT, SPST et de nombreux autres commutateurs DIP combinés classés selon les circuits. Nous vendons les commutateurs DIP et DIP rotatifs de grands fabricants. Choisissez vos commutateurs en affinant la recherche selon le nombre de positions, le type d’actionneur, le modèle de terminaison, le courant nominal, la tension nominale, etc.
What is a DIP switch? DIP Switches are manual electric switches that are packaged by group into a standard dual in-line package (DIP). This type of switch is designed to be used on a printed circuit board along with other electronic components to customize the behavior of an electronic device in specific situations. DIP switches are also known as toggle switches, which mean they have two possible positions -- on or off. (Sometimes instead of on and off, you may see the numbers 1 and 0 on the DIP Switch.)
There are many different kinds of DIP switches and at Future Electronics we stock many of the most common types including rotary, slide, and piano switches. We also offer a selection of DPDT dipswitches, SPDT dipswitches, low profile dipswitches, miniature dipswitches and micro-switches with extended actuator and flush actuators.
Rotary DIP Switches contain multiple electrical contacts. The way it is used is by rotating the switch to align it with a number printed on the package. These may be large like thumbwheels, or small enough to require a screwdriver.
The slide and piano types of switches, which are very common, are arrays of simple SPST (single-pole, single-throw) contacts. These can be either set in an on or off position allowing for each switch to have a one-bit binary value. The values of all switches in the DIP package can also be interpreted as one number. For example, seven switches offer 128 combinations, allowing them to select a standard ASCII character. Eight switches offer 256 combinations, which is equivalent to one byte and so on.
It’s really easy to hone in on the electric switch you need using our parametric filters. You can use them to quickly refine your Switch search results by switch operation, circuitry, termination style, actuator style, number of positions and package style.
DIP switch packages consist of socket pins or mounting leads to provide an electrical path from the switch contacts to the circuit board itself. While circuits can use these electrical contacts directly, it is more common to convert them into low and high signals. It’s important to note, in the case of a dipswitch that a circuit board also needs interface circuitry for the DIP switch to function. This can consist of a series of pull-up or pull-down resistors, a buffer, decode logic, and other components, which we offer at FutureEelctronics.com.
Typical Dip Switch applications include: Telecommunications, Computer Motherboards, Remote controls for frequency setting (like garage door openers) and other electronic devices requiring option settings. DIP Switches in R&D quantities or production ready packaging With our state of the art facility in Memphis and FutureElectronics.com, you have the option to order the exact number of dipswitches required for your R&D or electronic project needs without the unnecessary surplus of buying full reels or boxes dipswitches.