Manufacturer Part #
776428-2
DEUTSCH AMPSEAL 16 2 Position 4.5 mm Pitch Single Row Receptacle Housing
TE Connectivity 776428-2 - Product Specification
Shipping Information:
ECCN:
PCN Information:
General Description of Changes:The Industrial and Commercial Transportation business unit of TE Connectivity is making a change to assemble parts on the manual assembly line in addition to the automatic assembly line for the part numbers listed below. These PNs are TE proprietary designs, therefore considered catalog/general market product. PPAP and/or sample requests must be submitted within 14 days of PCN submission via ict-ppap-request@te.com or ePPAP system. Submission will not occur without request. If PPAP requested, disposition response is required within 14 days of submit date or it will be considered approved. Product drawing(s) are not affected.Reason for Changes:Dear Customer, we hereby inform you of this change. The change is necessary to increase our manufacturing capacity for AMPSEAL 16. The change does not impact connector performance. IMPORTANT: The current and previous revisions of these parts can be used interchangeably in the field. The changes are being phased in gradually and previous revision can remain stocked until use. Shipments of both configurations may be mixed.
Description of ChangesThe Industrial and Commercial Transportation business unit of TE Connectivity is introducing an additional manufacturing location in Suzhou, China for the part number(s) listed below. These PNs are TE proprietary designs, therefore considered catalog/general market product. PPAP and/or sample requests must be submitted within 14 days of PCN submission via ict-ppap-request@te.com or ePPAP system. Submission will not occur without request. If PPAP requested, disposition response is required within 14 days of submit date or it will be considered approved. Product drawing(s) are not affected.Reason for Changes:Dear Customer, we hereby inform you of this change. The new assembly line is necessary to expand the capacity to meet the current product demand. IMPORTANT: No fit, form, or function change. Parts of the new assembly line are identical to current production. Shipments from current and new tooling configurations may be mixed.
Description of Changes: Manufacturing location changeThe TE approved supplier for the AMPSEAL 16 wire (mat) seals currently molds those seals in the United States. This same supplier also molds the peripheral seals as well but at their China manufacturing facility where the mold was built. The supplier is planning to move the wire seal molds to their China manufacturing facility. The supplier built the wire seal molds in the US with ultimate plans to move the tooling to China where their primary manufacturing facility is located. By having the wire seal tools and the peripheral seal tools at the same manufacturing facility, stricter process and quality controls will become more efficient.
Description of Changes:Manufacturing location changeThe TE approved supplier for the AMPSEAL 16 wire (mat) seals currently molds those seals in the United States. This same supplier also molds the peripheral seals as well but at their China manufacturing facility where the mold was built. The supplier is planning to move the wire seal molds to their China manufacturing facility. The supplier built the wire seal molds in the US with ultimate plans to move the tooling to China where their primary manufacturing facility is located. By having the wire seal tools and the peripheral seal tools at the same manufacturing facility, stricter process and quality controls will become more efficient.
Part Status:
Available Packaging
Package Qty:
1 per Bulk