Manufacturer Part #
776492-1
DEUTSCH 14-18 AWG Gold Crimp Socket Contact
TE Connectivity 776492-1 - Product Specification
Shipping Information:
ECCN:
PCN Information:
Description of ChangesNOTIFICATION ONLY!!! This is a notice of packaging change which contains stamped product reels for shipping. This change is specific to the reel flange which holds the stamped product associated with this notification.Reason for Changes:Document clarification.Dear Customer, we hereby inform you about a change of packaging material. The reason for this change is to increase the integrity of the packing system. The change follows a strict procedure, which fully maintains quality, ability to supply and form-fit-function of the concerned products. The packaging implementation follows a certified quality management system in accordance with standard automotive requirements.
DESCRIPTION :-TE is notifying its customers of the installation of two new plating lines at the Pegg Road facility in Greensboro, North Carolina. TE is replacing an aged plating line and adding capacity to better serve TE s business and customer needs. The aged plating line was decommissioned and removed from use 10/31/2023. TE part testing and qualification will follow all standard guidelines to ensure the product coming off the new lines meets the same performance and quality as current production parts. If there are no responses to the PCN from the customers by 10/31/2024, TE will proceed based on the understanding the proposed PPAP submission is acceptable for the final approval by customer. The new plating lines will be installed and the estimated time for PPAP availability is 4/18/2025 with expected SOP 7/15/2025.REASON: Product improvement. TE is replacing an outdated plating line that has been in operation for 28 years. The plating technology advancement will allow TE to remove one aged plating line and replace it with two new plating lines which will increase capacity.
General Product Description: Heavy Duty Commercial Socket Assembly, Size 16, Stamped and Formed Description of Changes The Industrial and Commercial Transportation business unit of TE Connectivity is making a change to include a Tool ID mark for the part numbers listed below. These PNs are TE proprietary designs, therefore considered catalog/general market product. PPAP requests (no samples) must be submitted within 14 days of PCN submission via ict-ppap-request@te.com or ePPAP system. Submission will not occur without request. If PPAP requested, disposition response is required within 14 days of submit date or it will be considered approved. Product drawing are affected.Reason for Changes: Dear Customer, we hereby inform you of this change. The change is necessary for easy identification of the parts manufactured with the new capacity tooling. The change does not impact performance. IMPORTANT: The current and previous revisions of these parts can be used interchangeably in the field. Previous revisions can remain stocked until use, and shipments of both configurations may be mixed. Refer to PCN-21-106049 for more details regarding the new Capacity Tooling. Product Category: Geometry Change Feature: Label/Marking ChangeKind of Change: GeometryPotential Customer Impact: No Customer ImpactRemarks: Update Product Drawings to include Tool ID marking. Refer to PCN-21-106049 for more detailsFirst Ship Date of Changed Items (Changed Parts Only): 10-JUN-2022
Part Status:
TE Connectivity 776492-1 - Technical Attributes
Mounting Method: | Wire Mount |
Available Packaging
Package Qty:
4000 per Reel
Mounting Method:
Wire Mount