Manufacturer Part #
770520-3
AMPSEAL Series Socket Contact Gold 16-20 AWG Crimp Socket Terminal
|
|
|||||||||||
|
|
|||||||||||
| Mfr. Name: | TE Connectivity | ||||||||||
| Standard Pkg: |
Product Variant Information section
Available PackagingPackage Qty:5000 per Reel Mounting Method:Wire Mount |
||||||||||
| Date Code: | 2248 | ||||||||||
TE Connectivity 770520-3 - Product Specification
Shipping Information:
HTS Code:
ECCN:
PCN Information:
Kind of change: DrawingProduct Description:Ampseal Terminal Customer Drawing Block Tolerance UpdateGeneral Description of ChangesThe Industrial and Commercial Transportation business unit of TE Connectivity is making a minor drawing change to add back the block tolerance which was mistakenly removed in previous revisions for the product drawing(s).Reason for Changes:TE hereby inform you of this drawing change. The change is necessary to communicate correct tolerances for customer drawing dimensions. The change does not impac performance. IMPORTANT: There are no changes to parts as this is a documentation update only.First Ship Date of Changed Items (Changed Parts Only): 13-FEB-2026
Description of ChangesNOTIFICATION ONLY!!! This is a notice of packaging change which contains stamped product reels for shipping. This change is specific to the reel flange which holds the stamped product associated with this notification.Reason for Changes:Document clarification.Dear Customer, we hereby inform you about a change of packaging material. The reason for this change is to increase the integrity of the packing system. The change follows a strict procedure, which fully maintains quality, ability to supply and form-fit-function of the concerned products. The packaging implementation follows a certified quality management system in accordance with standard automotive requirements.
DESCRIPTION :-TE is notifying its customers of the installation of two new plating lines at the Pegg Road facility in Greensboro, North Carolina. TE is replacing an aged plating line and adding capacity to better serve TE s business and customer needs. The aged plating line was decommissioned and removed from use 10/31/2023. TE part testing and qualification will follow all standard guidelines to ensure the product coming off the new lines meets the same performance and quality as current production parts. If there are no responses to the PCN from the customers by 10/31/2024, TE will proceed based on the understanding the proposed PPAP submission is acceptable for the final approval by customer. The new plating lines will be installed and the estimated time for PPAP availability is 4/18/2025 with expected SOP 7/15/2025.REASON: Product improvement. TE is replacing an outdated plating line that has been in operation for 28 years. The plating technology advancement will allow TE to remove one aged plating line and replace it with two new plating lines which will increase capacity.
Description of Changes-TE is notifying its customers of the installation of two new plating lines at the Pegg Road facility in Greensboro, North Carolina. TE is replacing an aged plating line and adding capacity to better serve TE s business and customer needs. The aged plating line was decommissioned and removed from use 10/31/2023. TE part testing and qualification will follow all standard guidelines to ensure the product coming off the new lines meets the same performance and quality as current production parts. If there are no responses to the PCN from the customers by 10/31/2024, TE will proceed based on the understanding the proposed PPAP submission is acceptable for the final approval by customer. The new plating lines will be installed and the estimated time for PPAP availability is 4/18/2025 with expected SOP 7/15/2025.
Part Status:
TE Connectivity 770520-3 - Technical Attributes
| Mounting Method: | Wire Mount |
Features & Applications
The 770520-3 is a AMPSEAL 16-20 AWG Wire to Cable Crimp Socket Contact. It has an operating temperature range of -40 – +125 [-40 – +257].
The AMPSEAL connectors just got better. Known for their rugged reliability even under high-temperature automotive and industrial applications, they are now a snap to assemble. We have replaced the difficult-to-apply, labor-intensive gasket by bonding it to the header assembly. This product upgrade also eliminates purchasing and inventorying an extra part--the gasket. Or, if you prefer, we also offer the header with a separate gasket.
Features:
- Product Line = AMPSEAL
- Product Type = Contact
- Wire Insulation Diameter (mm [in]) = 1.70 – 2.70 [0.067 – 0.106]
- Contact - Rated Current (A) = 17
- Termination Method = Crimp
- Wire/Cable Size (AWG) = 16 – 20
- Contact Type = Socket
- Contact Termination Type = Crimp
- Contact Plating, Mating Area, Material = Gold
- Contact Base Material = Copper Nickel Zinc Alloy
Available Packaging
Package Qty:
5000 per Reel
Mounting Method:
Wire Mount