Référence fabricant
SIC437BED-T1-GE3
3 V to 28 V 12 A 1 Output Adjustable microBUCK® DC/DC Converter - PowerWFQFN-24
| | |||||||||||
| | |||||||||||
| Nom du fabricant: | Vishay | ||||||||||
| Emballage standard: | Product Variant Information section Emballages disponiblesQté d'emballage(s) :3000 par Reel Méthode de montage :Surface Mount | ||||||||||
| Code de date: | |||||||||||
Vishay SIC437BED-T1-GE3 - Spécifications du produit
Informations de livraison:
ECCN:
Informations PCN:
Description:No Physical, Process, or Location Changes We want to emphasize that products continue to be manufactured at the same locations, using the same equipment, materials, packaging, and process steps as before. There have been no changes to any aspect of the production process or sites involved.BackgroundThis alignment is part of a global initiative at Vishay to ensure consistent representation of CoO information across all divisions, based on international and national regulations, as well as World Trade Organization guidelines.Please NoteSome customers may have already noticed changes in the CoO information on documentation accompanying recent product deliveries. As part of this ongoing initiative, updates to the CoO may continue to appear over time in product documentation, where applicable. These changes align with the updated approach and do not reflect any physical changes to the products themselves.
Description of Change: Vishay is using a new PIQ material that is standard within our supply chain.Reason for Change: The PIQ vendor to our Foundry Partner has discontinued the PIQ material used on the below products. The replacement PIQ material is provided by the same vendor and is used in much greater volume of production.
Description of Change: The Mosfet wafer plating process and the Finish good Test for IC products will move to a new building within the same Laguna Technopark.Classification of Change: In order to increase capacity Vishay Siliconix has moved the Philippines wafer plating facility and the Final Test in a larger building with the same equipment, same process and same personnel.
Statut du produit:
Vishay SIC437BED-T1-GE3 - Caractéristiques techniques
| Méthode de montage : | Surface Mount |
Fonctionnalités et applications
Emballages disponibles
Qté d'emballage(s) :
3000 par Reel
Méthode de montage :
Surface Mount