Pays de livraison
Livraison gratuite aux États-Unis continentaux à partir de 50 $ US. Des conditions s'appliquent
Pays sélectionné
Un transistor est un dispositif semi-conducteur qui possède une partie solide et non mobile qui transfère une charge. Il peut amplifier et modifier les signaux électroniques et l'alimentation électrique, ce qui en fait un élément essentiel à de nombreux circuits. Feature Electronics propose plus de 12 000 émetteurs de grands fabricants. Explorez notre gamme de transistors bipolaires (BJT), transistors Darlington, transistors numériques, transistors à usage général, IGBT, JEFT et plus encore.
Découvrez des MOSFET Vishay PowerPAK® 8 x 8LR refroidis sur le de...
Les MOSFETs de puissance onsemi 80 V offrent un faible RDS(on), u...
Les transistors Infineon de 100 V GaN offrent une grande efficaci...
Featuring an optimized layout and higher current ratings, the Inf...
Total system solutions in the industrial power sector by ROHM, ha...
60 V automotive grade MOSFET family targeting 12 V and 24 V appli...
A transistor is a semiconductor containing a solid, non-moving part that passes a charge. A transistor can amplify and switch electronic signals and electrical power and is made of semiconductor material with at least three terminals that are used to connect to an external circuit. Transistors can amplify a signal because output power can be higher than input power. By applying a voltage or a current to one of the terminal pairs, there is a change in current through another pair of terminals.
There are several different kinds of transistors at Future Electronics. We stock many of the most common types categorized by several parameters including Polarity, Total Power Dissipation, Collector Current, CE Voltage, Packaging Type and many other parameters specific to the type of transistor. Our parametric filters will allow you to refine your search results according to the required specifications.
Future Electronics has a wide range of transistors from several manufacturers. Once you decide if you need Bipolar Transistors, Darlington Transistors, Digital Transistors, General Purpose Transistors, IGBT Transistors, JFETs or Load Switches, you will be able to choose from their technical attributes and your search results will be narrowed to match your specific transistor application needs.
There are many applications that use transistors including:
With the FutureElectronics.com parametric search, when looking for the right transistors, you can filter the results by category. We carry the following categories of transistors:
Once you choose the transistor category, you can narrow them down by various attributes: by Total Power Dissipation, Polarity, CE Voltage and Collector Current, to name a few. You will be able to find the right Darlington Transistors, Bipolar Transistors, Digital Transistors, IGBT Transistors, General Purpose Transistors, Load Switches or JFETs by using these filters.
If the quantity of transistors you require is less than a full reel, we offer to our customers several of our transistors in tray, tube or individual quantities that will help you avoid unneeded surplus.
Future Electronics also offers its clients a unique bonded inventory program designed to eliminate potential problems that may arise from an unpredictable supply of products that could contain raw metals and products with erratic or long lead times. Talk with your nearest Future Electronics branch and find out more on how you and your company can avoid possible shortages.